|
Web-Select Help & Info |
FCU Coil Alternatives
This is the third screen in Fan Coil Selection.
Coils displayed are based on selections in the previous two screens.
- General: Not an editable field.
- Unit Size:
- If Yes was chosen for Unit Size Known on Selection Screen 1,
Web-Select displays available coils that meet the criteria for the unit
size. Select the desired coil to make the selection.
- If No was chosen for Unit Size Known, Web-Select displays available
coils that meet the criteria, and all the unit sizes available for those
coils. Click on the radio button next to the desired coils to make
their selection.
After selecting the coils, click Next Step to continue.
See Also:
FCU Table of Contents
FCU Selection