|
Web-Select Help & Info |
Fan Coil Unit Pricing
Fan Coil Pricing consists of two input screens:
- Pricing Screen 1 is used when the
unit has not yet been Selected. It includes inputs for Tag, Model, Unit Size,
Coil 1, Coil 2. If Coil 1 and 2 are Water Coils, then Coil 1 GPM and Coil
2 GPM will appear as well.
- Pricing Screen 2 follows Pricing Screen
1 on non-selected units. For units that have been Selected, Pricing Screen
2 will be the screen displayed after clicking Price in the Product Schedule.
It includes inputs for Unit Information, Coil 1 and Coil 2 Options, and Unit
Options.
See Also:
FCU Selection
FCU Ordering