Web-Select Help & Info

Copying Web-Select Project Schedules Into a Spreadsheet

  1. Complete a Selection and Save To Schedule
  2. From the Project Information screen, click "View Schedule" for the appropriate Project.
  3. Click the Configure Custom Views button
  4. In the General Section, choose what columns should be displayed. If developing a submittal, uncheck the "Price", "View Pricing Results" and "Total Price" columns.
  5. When finished, name the Custom View in the "Custom View Management" area. If this is a new Custom View, click the New Custom View radio box. Then click the "Overwrite/Create/Delete" button.
  6. Once the Custom View is completed, click the small Print icon next to the Product Schedule drop-down menu. The next screen will display a clean Schedule with no links or buttons.
  7. Select the entire schedule, right-click and "Copy". Open the spreadsheet and Paste.
  8. Once imported into spreadsheet, copy from Column "C" to the end, then paste into another worksheet. This eliminates the check boxes, which will facilitate moving columns.

TIP: To keep the width of the schedule as small as possible, consider typing any redundant or secondary information as a note at the bottom of the Excel spreadsheet instead of including the column in the schedule. For example, "All motor voltages are 120/1/60".