ENVIRO-TEC Coil Selection Program

In addition to Web-Select®, ENVIRO-TEC offers a program for specialized coil selection: "ETI Coils." A website account is required to download the program.

  • ETI Coils includes coil data for SDL (single duct low height), VFL (parallel flow low height), and CFL (series flow low height) VAV coils. For fan coil and blower coil units, Web-Select is the preferred selection program; however, the ETI Coils program may be used for special circuiting and/or air temperatures above or below Web-Select limits.

Download now

Sitemap | Terms of Use| Privacy| Terms and Conditions
©2021 Johnson Controls