Web-Select Help & Info

Blower Coil Unit Coils

This is part of Blower Coil Selection Screen 2.  Available coils are based on input from Selection Screen 1.  Coil selections are the same for both Coil 1, Coil 2, and Reheat.  The following coils are available for blower coil units, depending on the model:

To clear all selections and return all fields to their defaults, click the Reset button.

See Also:
Unit Information
Unit Options
BCU Table of Contents
BCU Selection