Web-Select Help & Info

Blower Coil Unit Information

This is part of BCU Selection Screen 2.  Available choices are based on selections made in Screen 1.

To clear all selections and return all fields to their defaults, click the Reset button. When finished, click Next Step to proceed to Coil Alternatives.

See Also:
BCU Coils
BCU Unit Options
BCU Table of Contents