Web-Select Help & Info

Blower Coil Unit Coils

This is part of Blower Coil Pricing Screen 2.  The coils that appear here are dependent upon selections made in Pricing Screen 1.  Coil selections made are the same for both Coil 1 and Coil 2. 

The following coils are available for blower coil units, depending on model:

To clear all selections and return all fields to their defaults, click the Reset button.

See Also:
Unit Information
Unit Options