Web-Select Help & Info

Fan Coil Unit Coils

This is part of Fan Coil Selection Screen 2.  Available coils are based on input from Selection Screen 1.  Coil selections are the same for both Coil 1 and Coil 2.  The following coils are available for fan coil units, depending on the model:

To clear all selections and return all fields to their defaults, click the Reset button.

See Also:
Unit Information
Unit Options
FCU Table of Contents
FCU Selection