Web-Select Help & Info

Fan Coil Unit Information

This is part of FCU Selection Screen 2.  Available choices are based on selections made in Screen 1.

If the Selection Method chosen in Screen 1 was "Known CFM, Fan Speed, ESP", the following options will also display:

To clear all selections and return all fields to their defaults, click the Reset button. When finished, click Next Step to proceed to Coil Alternatives. 

See Also:
FCU Coils
FCU Unit Options
FCU Table of Contents